cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

My best guess would be time from I2C write to output pin valid.

But 2.485 ms for that seems horribly slow..

0 Likes
3 Replies
SampathS_11
Moderator
Moderator

2.485 ms is the worst case maximum IO Access time.

Thanks,

Sampath

0 Likes
Anonymous
Not applicable

Thanks for replying. But that doesn't define what "IO Access time" refers to...

- time for chip to ACK an I2C request....???

- time for chip to read a pin (and consequent response delay to an I2C read request)...?

- time for chip to write to pin (after having received a port set command)..??

- ...

0 Likes
SampathS_11
Moderator
Moderator

IO Access Time means

- time for chip to read a pin from start of I2C packet to end of I2C packet with clock stretching required to perform a port read

- time for chip to write to pin from start of I2C packet to end of I2C packet with clock stretching required to perform a port write

Thanks,

Sampath

0 Likes