cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

?What are the minimum requirements to program CY8C27443-24PXI AND CY8C29466-24PXI?

0 Likes
1 Solution
Bob_Marlowe
Expert II

The kit description shows that you can program the PSoC1 chips with the included Miniprog.

A Miniprog3 can be configured to program PSoC1 devices.

Nevertheless: Do consider to use a more modern PSoC4 as the CY8CKIT-043 Prototyping kit for very few money. It has inherent debug capabilities, runs on an ARM M0 CPU and the IDE (Creator 4.2) is downloadable at Cypress web site.

Bob

View solution in original post

4 Replies
Bob_Marlowe
Expert II

As IDE you'll need PSoC Designer 5.4

You may use a Miniprog or a Miniprog3 for programming. Be aware that there is no debugging capability except using an ICE for PSoC1

Consider using a more modern chip as a PSoC4 or PSoC5.

Bob

Anonymous
Not applicable

CYPRESS SEMICONDUCTOR  CY3210-PSOCEVAL1  Evaluation Kit, PSOC 1 SoC, MiniProg Programming Unit, LCD Module, Potentiometer, LEDs .Does this kit necessary to program the CY8C27443 AND CY8C29466 ? .Does Miniprog3 program CY8C27443 AND CY8C29466 ?

0 Likes
Bob_Marlowe
Expert II

The kit description shows that you can program the PSoC1 chips with the included Miniprog.

A Miniprog3 can be configured to program PSoC1 devices.

Nevertheless: Do consider to use a more modern PSoC4 as the CY8CKIT-043 Prototyping kit for very few money. It has inherent debug capabilities, runs on an ARM M0 CPU and the IDE (Creator 4.2) is downloadable at Cypress web site.

Bob

View solution in original post