I'm trying to wake the PSoC 5LP up from sleep mode using a comparator. For the reference I would like to use one of the DAC's, so that I can adjust the reference voltage before going to sleep.

What do I need to do to keep the DAC awake during sleep mode? Is this possible without using Alternative Active mode?

Here is an image of my TopDesign: http://i.imgur.com/ALhMYNK.png

0 Likes
5 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Welcome in the forum!

   

In sleep mode the DAC will be disabled, but the comparators will work. So you need to provide your required reference externally.

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

AltActive seems to imply yes (thru use of PM_STBY register write) -

   

 

   

   

 

   

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Tech support confirms AltActive will work -

   

 

   
Thank you for contacting Cypress Technical support.  Yes, the IDAC/VDAC can be active during the Alternate Active mode.   Regards, Dana.
0 Likes
Anonymous
Not applicable

 Something I have been wondering myself, is can Alt Active work just like sleep mode with the exception of one or two componets left online? Would the current draw be equal to SleepCurrent + OnlineDeviceCurrent?

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

There is more current drawn in alternate mode since most regulators stay active. To reduce pwr try to

   

use sleep and get woken up by comparator

   

or

   

use deep-sleep and get woken up by a pin. (might need an external comparator)

   

 

   

Bob

0 Likes