cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

chmoc_1567941
New Contributor

I want to sense voltage between 0 to 10 V from ADC with Circuit Divider??

   

My question is that where i connect my GND terminal of 0 to 10 V input with cypress??

0 Likes
3 Replies
Bob_Marlowe
Expert II

Your sensing voltage source and the PSoC board need to have a common ground GND.

   

 

   

Bob

0 Likes
chmoc_1567941
New Contributor

how can i do it??

   

may i connect 0 to 10 V GND with cypress GND??

   

or other psoc resource??

0 Likes
Bob_Marlowe
Expert II

may i connect 0 to 10 V GND with cypress GND??

   

Usually: Yes

   

But you may use a multimeter to see if there is a potential differenge between those two GND points

   

 

   

Bob

0 Likes