- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I am trying to measure a voltage over a resistor to get it´s value, my problem is that i can not calibrate the ADC to measure the correct voltage.
I tried to measure the offset manually as recommended in the AN84783 "Accurate Measurement Using PSoC 3 and PSoC 5LP Delta - Sigma ADCs" that gave me a value of 42942, which makes absolutely no sense, then i tried to calculate two known points into a function to eliminate offset and gain error, but that did not help either.
After that i tried to implement the two-point-calibration from the ADC-VoltageInp Example project, that does not help.
I think i did something basically wrong, could someone please take a look at my project and tell me where i screwed up?
I am using the CY8C5888LTI-LP097 Prototyping Board, and Creator 3.3, attached for you is a picture of my circuit that is on the breadboard now. I need to switch between the reference resistors to measure a bigger range of resistors. I measured the internal resistances from the PSoC and added them to the values, thats why they look so strange.
If you need further information please let me know, I hope i have translated all necessary comments in the SW into english.
Thanks for your help, Greetings, Patrick
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
You are not measuring the reference Voltage at pin V3out. Place an AMUX in front of ADC and swich the channels with a control register.
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Bob,
thank you for your advice, I tried to what you told me, the result is in the graphic attached, but I can´t get it working.
I tried to have the Vss in the ADC by enabling "Enable Vref/Vssa" and connecting it to ground over a pin, but that was not successful.
When i have a resistor of 2.7kOhms as Rx to measure the voltage over it the multimeter shows 3.755V and the ADC shows 3.763V. But the main Problem is that the voltage I am expecting is around 4.65V (Rx/Rx+Rref)*Ub = (2700/2700+200)*5V.
Where am I losing that voltage?
Thank you for your help, Greetings, Patrick
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
There is a resistor intern to the AMux switch, use the cydwr view, switch to analog and use the ohmmeter to estimate internal R
Bob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you for your help, i measured and corrected the values for the resistors.
For this test I did not use any corrections for the offset, etc, thats just the values directly from the ADC and the ADC_Del_CountsTo_uVolts(ADC_Del_GetResult32) -function.
The problem with the calibration still exists, when i point the wire from the ADC to ground (0V) it shows a value of 42949 and a voltage value of 4294967224 (that´s in µV so it would be 4294 V, that´s impossible!? ), is that some sort of a over/underflow? When i point the wire to Vdd it shows a value of 44431 and a voltage of 5.086721 V, even if Vdd is only 4.7V on the USB-Programming adapter.
Any Tips to get correct measurements?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
4294967224 is a 32bit uint, as an int32 it would represent the value -72 which is quite reasonable.
Your reference voltage is set to VDDA. You told (in .cydwr view/System) that it is 5.0V. So when it is not 5V (4.7) the conversion cannot be correct.
I would suggest you to
- Use the internal VRef of 1.024 V up to 6*VRef
- Bypass VRef on P0_3 with 1µF
- Change your input resistor ladder accordingly.
Bob