cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

  

   

Hi,

   

Iam new to PSOC devices. Iam using an CY8C5888 witch is a very cool device. I have played around with the USBUART component and I have noticed a strage behavior. When I plug the USB in my notebook docking station or USB hub then all works fine. But if I use one of the USB ports witch are located in my notebook then the Windows 7 tells my that there is a unknown device. The Vendor PID is 0 and Iam not able to install a driver. 

   

Dose anyone have a idea what could be the reason? (The USBUART example from the PSOC creator studio dose have the same behavior. )

   

thanks a lot for your answers! 

0 Likes
1 Reply
Bob_Marlowe
Expert II

Double post, answeres here www.cypress.com/

   

 

   

Bob

0 Likes