USBUART communication

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello there!
I have a problem with the USBUART component of psoc 5. I am sure that the serial communication is working properly when the COM is open (with open I mean that I have a SERIAL monitor open on the PC), but the whole code is stopped when the COM monitor is not open. So basically I have a perfect communication when the PORT is open, however when I close it everything is stopped. 

   

I would find a function which allows me to send data to the PC only when the communication "is open", thus allowing the code to run along while the COM port monitor is not open on the PC.

   

Any suggestions?

   

Thanks,

   

Matteo

0 Likes
1 Reply
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received
0 Likes