cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

I started getting this error when I build my project.

Build error: 'USBUART_MAX_EP' undeclared here (not in a function)

The error is in the USBUART_audio.h file. USBUART_MAX_EP is defined in USBUART.h.  I have not made any changes to to the API files.

0 Likes
3 Replies
AnkitaS_51
Employee

Is USBUART.h file included in the USBUART_audio.h file?

0 Likes
Anonymous
Not applicable

Thanks for your reply.  All of the required libraries are included.

I start out with a working USB UART application and then slowly add in my code, while testing along the way. After a while the compiler starts complaining. Sometimes it is intermittent and sometimes it fails repeatedly. If I hover over USBUART_MAX_EP , the IDE shows the value, so it can find it.  If I hard code the value at the problem statement, the error just moves to another similar error else where in the USBUART API.

One time, as a clean and build was running, I saw that the USB pins were reassigned (to the same ones I had assigned) and it compiled. I changed my my USB pins to "auto assign" and unchecked "lock". It now seems to regularly compile without any changes to the firmware???

I am not sure what is going on, but at least I was able to complete my firmware. I still have another test program that was not fixed by that trick, so it is not a magic bullet.

0 Likes
AnkitaS_51
Employee

Hello Bart,

Please provide us with your project with the issue.Which creator version are you using

0 Likes