cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

 I am using the psoc5.4 designer and created a project using an uart.

   

This project was working fine. Until I changed the paging attribute in the project settings.

   

My own code is only C I didn;t modify the assembler parts. 

   

So I may expect that the uart_1.asm and uart_1int.asm are correct and do support the LMM.

   

When Paging is enabled I see the UART_1_bRxCnt getting a value.

   

But the UART_1_aRxBuffer is filled with 0x00

   

What should I do to get the LMM working in combination with the uart.

0 Likes
9 Replies
Anonymous
Not applicable
        Hi Geert   
Which PSoC device did you use?   
LMM; I assumed it Cy8C29*** device.   
Where is use that UART API?   
In interrupt routine? or main polling loop?   
or both combined?   
   
Did you use context save and restore MACRO?   
like this in the interrupt routine   
... PRESERVE_CPU_CONTEXT   
... lcall _ISRC_TxComplete   
... RESTORE_CPU_CONTEXT   
0 Likes
Bob_Marlowe
Expert II
        Whenever possible upload your complete project here, using Designer's "Archive Project" function, so we all can have a look at your internal settings etc.   
   
Bob   
0 Likes
Anonymous
Not applicable

 I use the CY8C29666-24PVXI

0 Likes
Anonymous
Not applicable

 I do not use the PRESERVER_CPU_CONTEXT

   

The uart is interupt enabled. Receiving is done by interupt.

   

And in my C code I check the UART_1_bRxCont

   

In include uartc.h function  void uart_ontvangen(void)

   

I am however not able to debug with the ICE module. Because my psoc is togetter with other components in plastic.

   

So I can not connect to the psoc chip.

0 Likes
Anonymous
Not applicable
        Basically, In the interrupt routine RAM segment assign to Interrupt RAM area.   
That is first 256 byte, 0 - 255 byte.   
If your buffer area is place without interrupt RAM area,   
you can't access with it directly from interrupt routine.   
So, you have to call these save/restore MACRO.   
   
in_the_interrupt(void)   
{   
... PRESERVE_CPU_CONTEXT   
... lcall _ISRC_UserProcess ;; CALL USER PROCESS   
... RESTORE_CPU_CONTEXT   
}   
   
// USER CALL BACK ROUTINE //   
void ISRC_UserProcess(void)   
{   
// access your buffer   
... return;   
}   
0 Likes
Anonymous
Not applicable

 Do I need to modify the uart_1.asm or uart_1INT.asm for that ???

0 Likes
Anonymous
Not applicable

 I am not using an own (C code) Interup routine. So from the _UART_1_RX_ISR there is no call like you describe.
Maybe such a routine can be a workaround for my problem. (But then I need an example. how to implement such a routine.) 

   

Because I am just a beginner in PSOC development.

0 Likes
Anonymous
Not applicable

OK     

   

This is a real code of my Cy8C29466 – UART     

   

Something help for you.     

   

     

            

   

;-------------------------------------------------------     

   

; In the UARTINT.asm     

   

;-------------------------------------------------------     

   

_UART_RX_ISR:     

   

   ;@PSoC_UserCode_BODY_2@ (Do not change this line.)     

   

   ;     

   

   ;---------------------------------------------------     

   

   ; Insert a lcall to a C function below this banner     

   

   ;---------------------------------------------------     

   

   PRESERVE_CPU_CONTEXT     

   

   lcall _ISRC_RxReady     

   

   RESTORE_CPU_CONTEXT     

   

   ;---------------------------------------------------     

   

   ; Insert a lcall to a C function above this banner     

   

   ;---------------------------------------------------     

   

   ;@PSoC_UserCode_END@ (Do not change this line.)     

   

     

            

   

// ////////////////////////////////////////////////////     

   

// this is a user process in main.c     

   

// ////////////////////////////////////////////////////     

   

volatile byte RxFlag, RxIdx, RxLen;     

   

volatile byte RxBuf[UART_BUF_SIZE];     

   

// ////////////////////////////////////////////////////     

   

// in this routine, STX code 0x02 is start of record     

   

//    CR code 0x0D is end of record     

   

// this routine handle only text data 0x20 ~     

   

// ////////////////////////////////////////////////////     

   

void ISRC_RxReady(void)       // receive data ready     

   

{ byte ss;     

   

           

   

      if( (UART_bReadRxStatus()&UART_RX_REG_FULL) && !(UART_bReadRxStatus()&UART_RX_ERROR) )     

   

      {     ss= UART_bReadRxData();     

   

            if( ss==STX )                      

   

            {     RxIdx= 0;                     // if start text: clear pointer     

   

            }     

   

            else if( ss>=' ' )                  // if text data     

   

            {     RxBuf[RxIdx++]= ss;           //    set buffer     

   

                  if( RxIdx>=UART_BUF_SIZE-1 )  // if exceed data     

   

                  {     RxIdx= UART_BUF_SIZE-1;     

   

                        RxBuf[RxIdx]= 0;        // complete buffer     

   

                        RxLen= RxIdx;     

   

                        RxIdx= 0;     

   

                        RxFlag= 1;              // record comleted     

   

            }     }          

   

            else if( ss==CR )                   // if end of text     

   

            {   if( RxIdx )     

   

                  {     if( RxIdx>=UART_BUF_SIZE-1 ) RxIdx= UART_BUF_SIZE-1;     

   

                        RxBuf[RxIdx]= 0;        // complete buffer     

   

                        RxLen= RxIdx;     

   

                        RxIdx= 0;     

   

                        RxFlag= 1;              // record comleted     

   

      }     }     }     

   

}     

   

     

            

   

// ///////////////////////////////////////////////////////////////////     

   

void UART_Initialize(void)     

   

{   UART_Start(UART_PARITY_ODD);      // Parity Odd       

   

    UART_EnableInt();     

   

    UART_IntCntl(UART_ENABLE_RX_INT); // Enable RX interrupts     

   

}     

   

     

            

   

// ///////////////////////////////////////////////////////////////////     

   

byte UART_Receive( byte rec[], byte siz )     

   

{ byte len;     

   

      if( !RxFlag ) return 0;     

   

      if( siz>=UART_BUF_SIZE-1 ) siz= UART_BUF_SIZE-1;       

   

      len= RxLen;     

   

      RxLen= 0;     

   

      if( siz<len ) len= siz;     

   

      strncpy( rec, (char*)RxBuf, len );     

   

      RxFlag= 0;     

   

      return len;       

   

}     

   

     

            

   

// ///////////////////////////////////////////////////////////////////     

   

int main(void)     

   

{ byte ss, rec[UART_BUF_SIZE];     

   

     

            

   

UART_Initialize();     

   

    M8C_EnableGInt;         // enable global interrupts     

   

     

            

   

      While(true)     

   

{     if( ss=UART_Receive(rec, UART_BUF_SIZE) )     

   

            {     

   

              // do something using rec[]     

   

      }     }     

   

}          

   

// ///////////////////////////////////////////////////////////////////     

   

     

            

0 Likes
Anonymous
Not applicable
        Thanks for your support and for the sample code. I found already that the issue I have is not memory model related.   
0 Likes