- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I want to use the Delay10msTimes function from the article here http://www.cypress.com/?id=4&rID=47960 .
I unzipped the delay.asm and delay.h files and included them in my project. I included the .h file using the "#include <delay.h>" line of code.
The code in the "delay.h" won't compile. I get the following warnings & errors:
WARNING: DELAY.H:12: unknown #pragma, line ignored
WARNING: DELAY.H:13: unknown #pragma, line ignored
WARNING: DELAY.H:14: unknown #pragma, line ignored
ERROR: DELAY.H:19: syntax error near 'Multiple', expected ')'
ERROR: DELAY.H:20: syntax error near 'TenMstimes', expected ')'
I want to create a 1 second pulse on a pin. I was going to do this with the following code:
Timer_Reset_1_Write(1); //Set the PIN High
Delay10msTimes(100); //Wait 1 second
Timer_Reset_1_Write(0); //Set the PIN Low
- Labels:
-
PSoC 3
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
As mentoined by lkoziarz the Knowledge base article is related to PSoC1. For PSoC3 however the delay functions are generated by PSoC Creator. The functions include:
- CyDelay(uint32 milliseconds), that generates delay in multiples of milliseconds
- CyDelayUs(uint16 microseconds), that generates delay in multiples of microseconds
- void CyDelayCycles(uint32 cycles), Delay by the specified number of cycles using a software delay loop.
- void CyDelayFreq(uint32 freq) , Sets clock frequency for CyDelay.
The references and explanation for the same can be found in the "System Reference Guide". The same can be accessed from PSoC Creator, Help --> Documentation --> System Reference Guide.
The definitions for these functions in PSoC creator can be found in "CyLib.c".
-U2
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks for clarifying the subroutine names, I was going from memory. When you get that version of PSoC Creator for Linux ready, it will be quicker for me to have it handy all the time... 😃
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you for the responses. If I were to implement the same delay in PSoC5 I would then need to look at the System Reference Guide in order to find the appropriate function and header file?