Temperature range

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
pacr_284376
Level 5
Level 5
100 replies posted 10 solutions authored 50 sign-ins

 Hi there

   

I would like to use a PSOC 3 device (48 pins or more) which has a temperature range of upto 125°C. I only see the SSOP-48 and 100-TQFP packaged supported. Are there plans for other packages (48/64-QFN) planned in the near future to support this temperature range ?

   

Thanks

   

 

   

Patrick

0 Likes
3 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

On top of this page enter "PSoC3" into the Part Search field. You'll get a list of all PSoC3s. When you click on the temperature range the -40° to 125° will be listed first.

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Based on device selector in Creator thats all I found. Consider

   

filing a CASE and asking that question -

   

 

   

    

   

         

   

To create a technical case at Cypress -

   

 

   

www.cypress.com

   

“Support”

   

“Technical Support”

   

“Create a Case”

   

 

   

You have to be registered on Cypress web site first.

   

 

   

Regards, Dana.

   

 

   

0 Likes
pacr_284376
Level 5
Level 5
100 replies posted 10 solutions authored 50 sign-ins

 Thanks for the answers,

   

I created a CASE for this

0 Likes