cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Aswinpk94
New Contributor

I am performing Square wave voltammetry using PSoC 5LP. In it, a square wave is superimposed on a base staircase potential. It is then applied to an electrochemical cell with a 3 electrode configuration. I have generated a waveform. Now I want to test it before applying it to the cell. I need to perform both DC and AC analysis of the circuit. Does anybody have any suggestions?

Experiment conditions: Potential range: -1 to +1V. Width of pulse: 25ms. Max current to be sourced at the cell: 100 microAmps(0.1mA).

Perform AC analysis on different time constants and measure current

 Steady state DC AnalysisSteady state DC AnalysisTest circuitTest circuitAC analysis schematicAC analysis schematicSquare+staircaseSquare+staircaseand share your views on the schematic I shared with this?

0 Likes
3 Replies