Announcements
IMPORTANT: Cypress Developer Community currently doesn’t allow sign-in to prepare for the upcoming transition. To learn more, check out our announcement.
cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

Hi,

   

To estimate the minimum sampling frequency that could be used for S/H (Sample and Hold) module in PSoC 3/5,
we need to know the droop rate of the S/H circuit. Droop rate of the S/H circuit
refers to the rate at which the voltage across the hold capacitor(inside the S/H)
drops with respect to time in hold mode.However, the droop rate of the S/H module is not characterized.

   

I have attached two projects “sample_hold_test” and “sample_SH” that can be used for estimating the maximum hold time and minimum sample speed for 10% voltage droop respectively.
The same projects could be reused by minor modifications in the firmware for different voltage tolerances.

   

All the tests were done on CY8CKIT-030 PSoC3 DVK.

   

I hope this would help for those looking for S/H droop rate.

   

S

0 Likes
1 Reply
ETRO_SSN583
Esteemed Contributor

Just a couple of suggestions -

   

 

   

1) Show people how to compute, for a given resolution, the necessary max droop rate.

   

For example, if max A/D in = 2.5V, resolution 16 bits, then droop should be < 2.5 / 2**17

   

for 1/2 lsb max droop error.

   

 

   

2) Also in comments suggest the importance of temp, what the source of leakage is,

   

and how it behaves.

   

 

   

Regards, Dana.

0 Likes