Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
docn_292601
Level 2
Level 2
10 replies posted 10 sign-ins 5 replies posted

config:

   

   

 

   

my test code:

   

SPIM_3_Start();
    while(1)
    {
        SPIM_3_TxEnable();                           //使能SPI发送
        SPIM_3_ClearRxBuffer();                      //清空Rx缓存
        a = SPIM_3_GetRxBufferSize();
       
        SPIM_3_WriteByte(READ_SECOND_REG);           //发送地址
        SPIM_3_TxDisable();
        while(!(SPIM_3_ReadStatus() & SPIM_3_STS_TX_FIFO_EMPTY));
        b = SPIM_3_GetRxBufferSize();
       
        //使能SPI接收
        c = SPIM_3_GetRxBufferSize();
       
        while(!(SPIM_3_ReadStatus() & SPIM_3_STS_RX_FIFO_NOT_EMPTY));
        e = SPIM_3_GetRxBufferSize();
        d = SPIM_3_ReadByte();                       //读出数据
       
        sprintf(msg,"TIME:  %d %d %d  %d %d",a,b,c,d,e);
        draw_debug(msg,0,0);
    }

   

 

   

who  can tell me that the datas i get from DS1302 always are 0xff ???

   

thank you!!!

0 Likes
1 Solution
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Another issue I just see:

   

Before switching from transmit to receive you check the TxStatus for FiFo empty, but you should wait for complete transmission since the pin will switch to input before the transfer is complete.

   

 

   

Bob

View solution in original post

0 Likes
9 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

SPIM_GetRxBufferSize() only returns the number of characters, not the characters itself.

   

You ought to read the RxStatus until there is a byte in the buffer and then get it.

   

You just posted part of your code and part of the settings, so we cannot check everything. To post the complete project use the "Create workspace Bundle" of Creator and upload the .zip archive using ms internet explorer (NOT CHROME!!!)

   

 

   

Bob

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Another issue I just see:

   

Before switching from transmit to receive you check the TxStatus for FiFo empty, but you should wait for complete transmission since the pin will switch to input before the transfer is complete.

   

 

   

Bob

0 Likes
docn_292601
Level 2
Level 2
10 replies posted 10 sign-ins 5 replies posted

now:

   

SPIM_3_Start();
    while(1)
    {
        SPIM_3_ClearRxBuffer();
        SPIM_3_ClearTxBuffer();
        SPIM_3_TxEnable();
        SPIM_3_WriteByte(0x81);
        while(!(SPIM_3_ReadStatus() & SPIM_3_STS_TX_FIFO_EMPTY));
        SPIM_3_TxDisable();
       
        while(!(SPIM_3_ReadStatus() & SPIM_3_STS_RX_FIFO_NOT_EMPTY));
       
        a = SPIM_3_GetRxBufferSize();
        b = SPIM_3_ReadByte();
        sprintf(msg,"TIME:  %d  %d",a,b);
        draw_debug(msg,0,0);
    }

   

this does not work ,too.

   

the result is  a = 1, b = 255.

0 Likes
docn_292601
Level 2
Level 2
10 replies posted 10 sign-ins 5 replies posted

can you give me a example of SPI in SPI Bidirectional Mode???

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Your code still checks the fifo and not the completeness of transfer.

   

This is your code

   

        while(!(SPIM_3_ReadStatus() & SPIM_3_STS_TX_FIFO_EMPTY));
SPIM_3_TxDisable();

   

Better check for

   

Bob

   

   

SPIM_3_STS_SPI_DONE

0 Likes
docn_292601
Level 2
Level 2
10 replies posted 10 sign-ins 5 replies posted

ok , i will check it on Monday.

   

as you said, it is better .you are not sure it is right.

   

i will try it.

   

thank you very much.

   

谢谢.

0 Likes
docn_292601
Level 2
Level 2
10 replies posted 10 sign-ins 5 replies posted

it does not work ,too.

   

i went to my Master Shifu.

   

he tested  the SPI bidirection(3-wire) mode.

   

finally, he wrote these codes:

   


SPIM_3_Start();
    while(1)
    {
        SPIM_3_ClearRxBuffer();
        SPIM_3_ClearTxBuffer();

   


        SPIM_3_TxEnable();

   


        SPIM_3_WriteByte(0x81);     //read the second reg from the DS1302

   

        SPIM_3_WriteByte(0x81);    //call again,just  for txtending the clk and ss singal and waiting the back datas.

   

        while(!(SPIM_3_ReadStatus() & SPIM_3_STS_RX_FIFO_NOT_EMPTY));
      
        SPIM_3_TxDisable();
       
        a = SPIM_3_ReadByte();
        b = SPIM_3_ReadByte();
        sprintf(msg,"  %d  %d",a,b);
        draw_debug(msg,0,0);
    }

   

the result: a = 129  (0x81)                b is a right value from the DS1302

   

 

   

now  i am Confused, i can not  write the reg of DS1302.

   

even i add the code (eg.  SPIM_3_WriteByte(dat) )after SPIM_3_TxEnable()     i will not get the right b.

   

i can not find  an example of SPI bidirection(3-wire) mode, can you send me one.

   

thank you.

0 Likes
Anonymous
Not applicable

I used to use 4 wire mode, but try the following if that works

   

 

   

   

Please noted

   

The 1st byte to ds1302 is different for read and write operation

   

   

SPIM_3_WriteByte(0x80);     //WRITE TO 1ST REGISTER OF THE DS1302!!!!

   

And 

   

SPIM_3_WriteByte(0x81);     //READ THE 1ST REGSITER FROM THE DS1302!!!!

   

 

   

****************

   

1. To write ds1302

   

   

SPIM_3_ClearRxBuffer();

   

SPIM_3_ClearTxBuffer();

   

SPIM_3_TxEnable();

   

SPIM_3_WriteByte(0x80);     //write to 1st register of the DS1302

   

while(!(SPIM_3_ReadStatus() & SPIM_3_STS_SPI_DONE));

   

SPIM_3_WriteByte(SendData);    

   

while(!(SPIM_3_ReadStatus() & SPIM_3_STS_SPI_DONE));

   

 ************************

   

2. To read ds1302

   

 

   

SPIM_3_ClearRxBuffer();

   

SPIM_3_ClearTxBuffer();

   

SPIM_3_TxEnable();

   

SPIM_3_WriteByte(0x81);     //read the 1st regsiter from the DS1302

   

while(!(SPIM_3_ReadStatus() & SPIM_3_STS_SPI_DONE));

   

SPIM_3_TxDisable();

   

   

SPIM_3_ReadByte(); /* a dummy one, just to have the slave shift data out */    

   

returnData = SPIM_3_ReadByte(); 

   

   

 *****************

   

See if this works

0 Likes
docn_292601
Level 2
Level 2
10 replies posted 10 sign-ins 5 replies posted

i will try another day.

   

i have given up the SPI  module, now i use the PINs to write and read the DS1302.

0 Likes