cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

 Hi,

   

i need some rtos functionality for an embedded application. Through having keil c51 there is rtx51tiny included.

   

I already built a project using rtx51 but there seems to be problems with the timer 0 interrupt. Task switching os only done with explicitely calling os_switch_taks(). Self switching and os_wait does not seem to work.

   

 

   

I found, that there was an application note (AN64429.pdf) which couldn't be found anymore.

   

 

   

Would anyone b so kind to upload this file?

   

 

   

Thank

0 Likes
4 Replies
Anonymous
Not applicable

Hi abnoname,

   

 

   

The application note is attached along with this post.

0 Likes
Anonymous
Not applicable

 Oh many thanks for your fast response 🙂

   

 

   

As I see it would be helpfull to have the example project as well.

   

 

   

Is it possible to upload it too? Would me help so much.

   

 

   

Thanks.

0 Likes
Anonymous
Not applicable

Yup, uploading the project too.

   

Please note that it is not updated with the latest components.

0 Likes
Anonymous
Not applicable

Thanks 🙂

   

Now it works as expected.

   

Will this component become official into the next releases?

0 Likes