Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 5, 3 & 1 Forum Discussions

MaCa_285251
Level 1
First like given
Level 1

Hi everybody,

   

I'd like to use the RefMux module on a CY8C28623 to route signals to the analog output bus.

   

When I place the RefMux (v1.3 in PSoC Designer 5.4) I don't see any link appearing between the AnalogColumn_InputSelect multiplexer and the RefMux itself, as it happened using other PSoCs like CY8C27443 for example.

   

Furthermore the RefMux v1.3 datasheet doesn't report the CY8C28623 in the list of compatible devices: CY8C29/27/24/22xxx, CY8C23x33, CY8CLED02/04/08/16, CY8CLED0xD, CY8CLED0xG, CY8CTST120, CY8CTMG120, CY8CTMA120, CY8CTST300, CY8CTMA300, CY8C28x45, CY8CPLC20, CY8CLED16P01, CY8C28x43.

   

So I would like to know if I can use this module and which is the correct way to do it with CY8C28623.

   

Many thanks in advance.

   

Marco

0 Likes
7 Replies
Bob_Marlowe
Level 10
First like given 50 questions asked 10 questions asked
Level 10

Are you mistaking RefMux and AMUX ?

   

Bob

0 Likes
ETRO_SSN583
Level 9
100 sign-ins 5 likes given 1000 replies posted
Level 9

Looks like the P/N not in datasheet a simple omission. If RefMux placed code

   

is generated for its API's and definitions, eg, looks like it is a normal accessable

   

component/module for the 28xxx series of parts.

   

 

   

I concur with Bob, RefMux does not "feed" the column mux, you are thinking of

   

AMUX.

   

 

   

Regards, Dana.

0 Likes
MaCa_285251
Level 1
First like given
Level 1

Dear Bob and Dana,

   

thank you for your replies, I'm referring to RefMux.

   

As reported in the datasheet the RefMux can be used to provide "... a method to route external analog inputs directly to the analog output bus" (from the datasheet), by selecting the PMuxOut input.

   

The attachment "RefMuxPlacement.jpg" report the use of RefMux in a CY8C27443 project where you can see the link between the analog mux output and the RefMux input; if I use the CY8C28623 this link can't be established, maybe it is only a "graphical" issue.

   

 

   

Please let me know your opinion.

   

 

   

Regards,

   

Marco

0 Likes
Bob_Marlowe
Level 10
First like given 50 questions asked 10 questions asked
Level 10

There is no connection between an input pin of port0 to the RefMux output and analog buf. You only may select from the sources from the list. The connection is as unusable as the clock source selection for a column connected to a ctb (upper row). When you want to route different pins to the output buffer, use a PGA gain 1.0 and make the appropiate connections.

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
100 sign-ins 5 likes given 1000 replies posted
Level 9

Yes, using the PMUXout input to the RefMux one of 4 pins can be routed

   

direc tly to the analog output buffer. I also concur that one cannot

   

"see" the route.

   

 

   

The RefMux User Module switches one of three internal references (AGND, REFLO, or REFHI) to the analog output bus. Additionally, the output of the Continuous Time (CT) block PMux multiplexer can be selected. The RefMux User Module makes use of the TestMux in a CT block. These signals may be routed to a switch capacitor block on the bottom analog row or buffered and routed to an external pin. If used in conjunction with the AMux4 User Module, they form a four input analog multiplexer to route signals from one of four pins to the analog output bus.

   

 

   

Figure 1. RefMux Block Diagram

   

 

   

0 Likes
ETRO_SSN583
Level 9
100 sign-ins 5 likes given 1000 replies posted
Level 9
        
  • Low voltage offset path from PMux to analog output bus
  •     
  • Provides a method to route internal references (AGND, REFHI, REFLO) to an external pin
  •     
  • Provides a 4 to 1 analog mux for switch capacitor blocks such as ADCs and filters, if used with the AMux4 User Module
  •     
  • Signals from PMux through test mux may be rail-to-rail
  •     
  • Provides a method to route external analog inputs directly to the analog output bus
  •    
   

 

   

Be carefull regarding the statement about R-R performance. That is true until you pass

   

thru the output buffer, then a combination of its CM input range and output CM range

   

destroy all R-R performance.

   

 

   

Regards, Dana.

0 Likes
MaCa_285251
Level 1
First like given
Level 1

Dear Dana, thank you for your reply.

   

 

   

Regards,

   

Marco

0 Likes