Reducing size for PLC circuit

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Dear All,

I’m developing a PLC system based on CY8CPLC10.

I bought a couple of evaluation boards to make them communicating and everything seems to be ok.

Now I’m designing my own board for my application, following the information that I found in the Zip file “CY3273 Board Design Files (Schematic, Layout, Gerber, BOM)” download from Cypress web site.

My application is slightly different from the standard one: I use PLC on battery cables with voltages that may vary from 15Vdc to 150Vdc depending on the type of battery is installed on (anyway I tested the application with the evaluation boards and it works).

Unfortunately I have not a lot of area where to put the circuits and I need to reduce the size of critical components as much as possible. So, finally, my questions are:

  • Can I substitute the 1:1 transformer with a smaller one? In the Zip file you proposed for T1 the component “Precision Components 0505-0821G”. Could you propose a smaller one or tell me the minimum requirements for this component?
  • Can I substitute C9 “Panasonic ECQ-U3A154MG” with a smaller one, considering that I don’t need to connect the application to a 230Vac line but to a 150Vdc line? Is it mandatory to use a polypropylene capacitor or can I use other technologies, like ceramic or polyester or other?

I look forward to your kind reply.

Alberto.

PS: I'm not sure I'm posting the question in the proper area, but I wasn't able to find a specifica area for PLC. In case, please let me know for future questions.

0 Likes
1 Solution

Hello Alberto,

I request you to kindly refer to AN55427 - Cypress Powerline Communication Board Design Analysis for component guidelines.

Section 2.3 would be relevant to your questions,

pastedImage_0.png

Thanks,

Sampath

View solution in original post

0 Likes
3 Replies
SampathS_11
Moderator
Moderator
Moderator
250 sign-ins 250 solutions authored 5 questions asked

Hello Alberto,

I think you are referring to " CY3274 (Designer, Programmer, Kit Design Files, Examples, Documentation).zip"

- You can make use of a smaller transformer for T1, as long as you make enough margin for the maximum bus voltage, which, in your case is 150V

- You can make use of a capacitor with a lower voltage rating, leaving enough margin to suit your system design and safety requirements

Thanks,

Sampath

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Dear Sampath,

thank you for your reply.

In particular I’m referrig to “CY3272 Board Design Files (Schematic, Layout, Gerber, BOM)”, here enclosed.

I gently ask to give me more detail regaring the issues below:

- Regarding the transformer, should I mind some parameters like the primary inductance, V*usec product, max ESR?

- Regarding the capacitor, any technolgy is suitable for the application? Is the capacity value critical? Should I grant max ESR/ESL?

- Can I use, for example, Pulse PA0184NLT and Panasonic ECQ-E2154KF?

I look forward to your kind reply.

Best Regards,

Alberto.

Da: Sampath Selvaraj

Inviato: lunedì 9 luglio 2018 10:14

A: Alberto Ferrero <a.ferrero@atonstorage.com>

Oggetto: Re: - Reducing size for PLC circuit

<http://www.cypress.com/>

<https://community.cypress.com/?et=watches.email.thread> Cypress Developer Community

Reducing size for PLC circuit

reply from <https://community.cypress.com/people/samp?et=watches.email.thread> Sampath Selvaraj in PSoC 1 - <https://community.cypress.com/message/162129?et=watches.email.thread#162129> View the full discussion

0 Likes

Hello Alberto,

I request you to kindly refer to AN55427 - Cypress Powerline Communication Board Design Analysis for component guidelines.

Section 2.3 would be relevant to your questions,

pastedImage_0.png

Thanks,

Sampath

0 Likes