Hi! I'm trying to transfer example code (CE85976) for CY8C22545-24AXI controller(it uses SmartSense2X) into CY8C20536A-24PVXI controller(it uses general SmartSense). It needed to turn on and off 3 leds with 3 sensors. Use PSoC Designer 5.4.

   

 

   

The compiler tells me, that identifier "SmartSense_bScanComplete" is undeclared. Line editor doesn't know such an identifier at all. May be I can substitute it with something similiar? There is the part of the code:

   

 

   

while(1)
    {
   
        if(scanningFlag==SCAN_FIRST_SENSOR)
        {
               
            capSensorNo=0 ;   // initializing to scan first sensor
            SmartSense_ScanSensor(capSensorNo);
            scanningFlag= FIRST_SENSOR_SCAN_DONE; 
           
        }
        else if(scanningFlag == FIRST_SENSOR_SCAN_DONE)
        {
            if(SmartSense_bScanComplete & SmartSense_SCAN_COMPLETE)   //checking for sensor scan is complete

   

     {

   

   SmartSense_bScanComplete &=    ~SmartSense_SCAN_COMPLETE ;   // clearing the sensor scan complete flag
                SmartSense_UpdateSensorBaseline(capSensorNo); // Run baseline filter
                SmartSense_bIsSensorActive(capSensorNo);    // updating the SmartSense_baSnsOnMask[]
           
                capSensorNo++;   // increment to scan next sensor

0 Likes
1 Reply
Anonymous
Not applicable

Problem solved, I found programming guide for C compiler.

0 Likes