cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

GuNo_288966
Contributor

Hi,

   

can a PSoC5LP be a LIN master? There is a LIN component, but this seems to be a slave only.

   

The LIN protocol seems to be relatively slow, e.g. 19200bps. Does anyone have experience with LIN and is willing to share?

   

Best regards,

   

Turtle

   

Addition:

   

In the mean time I found out that there is a component named LIN USART in some PSoC1 that can be used as a LIN master.

   

As far as I understood is the problem the main problem the synchronisation gap at the beginning that is longer than a byte sent by the UART so that the UART can not generate this signal. Shouldn´t it be possible to use a AND to combine a control register bit and the UART output to generate this sync gap?

   

I have to send only one constant packet to make one sensor reply.

0 Likes
2 Replies