- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello!
I'm trying to implement a few of the Self-Test functions from AN78175 into an existing project that requires testing of the SRAM at runtime.
I started with the workspace included in AN78175. After removing the custom linker script which was calling out a non-existent "micro-names.inc" include file (see here), the project compiled just fine for a CY8CKIT-050 and the SelfTests_SRAM_March() and SelfTests_SRAM_Checkerboard() functions appear to work fine and the SRAM checks out as OK.
Where I'm running into a problem is using the Self Test SRAM functions in my own project for a CY8C5667AXI-LP040. Using the example project code as a guide, I created tests for both Flash (using ECC, seems to work OK) and a SRAM test function, which is what I'm having an issue with:
bool Perform_SRAMTest (void){
uint16_t init_marchcounter = 0;
uint8_t result;
/* Initialize RAM base address for checkerboard test */
SelfTests_Init_SRAM_Test();
/* Initialize RAM base address for March test */
SelfTests_Init_March_SRAM_Test();
/***************************************/
/* Run March RAM Self-test */
/***************************************/
/* Wait for end of SRAM test */
result = SelfTests_SRAM_March();
printf("R:%d\r\n",result);
init_marchcounter++;
while((result != PASS_COMPLETE_STATUS) && (init_marchcounter != NUMBERS_OF_TEST_CYCLES))
{
result = SelfTests_SRAM_March();
printf("R:%d\r\n",result);
init_marchcounter++;
}
if(init_marchcounter == NUMBERS_OF_TEST_CYCLES)
{
/*error*/
DBG_UART_PutString("SRAM MARCH ERROR\r\n");
return true;
} else {
DBG_UART_PutString("SRAM MARCH PASS\r\n");
return false;
}
}
This should be functionally identical to the example project, but with some printf() calls to track the result of each call of SelfTests_SRAM_March(); I am finding that every call results in a result of 1. I have also tried using SelfTests_SRAM_Checkerboard(WORDS_IN_BLOCK); but that also returns error status.
So unless the SRAM in this part is bad (unlikely) I must have done something wrong, or maybe I need to adjust something for the change in part from a CY8C5868AXI-LP035 to a CY8C5667AXI-LP040? What might I be missing here?
I have made and attached a test project that exhibits the problem for CY8C5667AXI-LP040. It performs a SRAM test and a FLASH test using ECC and spits the result out via UART. There's only a few components (a few IO pins, a timer, and a status register). It at least tells me that it's probably unrelated to any of my code in the large project.
Any tips would be greatly appreciated!
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Well I found some addresses in the project that didn't line up with the .map file and cydevice.h. Going to go over them one by one.
First, the stack. The original starting address for the stack is defined as:
/* Start address of Stack */
.equ CYDEV_STACK_BASE_H, 0x2000
.equ CYDEV_STACK_BASE_L, 0x7800
/* End address of Stack */
.equ END_STACK_ADDR_H, 0x2000
.equ END_STACK_ADDR_L, 0x8000
Looking in the .map file for the actual build, this did not match the actual placement:
.stack 0x20003800 0x800
0x20003800 __cy_stack_limit = .
0x20004000 . = (. + 0x800)
According to the map file, I should be setting up at 0x20003800-0x20004000 like so:
/* Start address of Stack */
.equ CYDEV_STACK_BASE_H, 0x2000
.equ CYDEV_STACK_BASE_L, 0x3800
/* End address of Stack */
.equ END_STACK_ADDR_H, 0x2000
.equ END_STACK_ADDR_L, 0x4000
I also looked into the other addresses. Next is the SRAM Base Address:
/* Address of SRAM base */
.equ CYDEV_SRAM_BASE_H, 0x1fff
.equ CYDEV_SRAM_BASE_L, 0x8000
Looking in cydevice.h, this did not line up with the actual SRAM starting address of the device:
#define CYDEV_SRAM_BASE 0x1fffc000u
#define CYDEV_SRAM_SIZE 0x00008000u
So I changed the SRAM Base Address to match cydevice.h:
/* Address of SRAM base */
.equ CYDEV_SRAM_BASE_H, 0x1fff
.equ CYDEV_SRAM_BASE_L, 0xC000
With this change made, the SRAM testing area also needed to change, since our ending address of SRAM is not 0x20007800 as it is in the original project, but is 0x20004000 going by cydevice.h:
(CYDEV_SRAM BASE + CYDEV_SRAM_SIZE)
(0x1FFFC000 + 0x00008000) = 0x20004000
The reserved SRAM must be at the end of the SRAM, but since that's where the stack is, I'm figuring I need to place just before the stack. That would put the reserved section at 0x20003400-0x20003800.
So I adjusted the reserved SRAM section:
/* Block size in SRAM test */
.equ BLOCK_SIZE_BYTE, 0x0400
/* Reserved part of SRAM used for RAM data storing during the March test. */
/* Reserved area is 0x20007000 - 0x20007400. */
.equ START_BUFF_ADDR_H, 0x2000
.equ START_BUFF_ADDR_L, 0x7000
.equ END_BUFF_ADDR_H, 0x2000
.equ END_BUFF_ADDR_L, 0x7400
After these changes, the march test now passes in my test project. All told it looks like I just had to adjust the SRAM addresses to match the changes in SRAM between devices (for some reason I thought this was an automated thing and it would utilize the generated constants from cydevice.h). Now hopefully porting this over to my actual project will be a smooth endeavor.