- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Seldom have issues with SPI, just plug and go.
This time have a SPI bi-directional master at a lowly 3Mbps. Leave it in transmit mode until need to turn it around.
Was occasionally getting hang ups with the slave. Hooked up an analyzer on the downstream data and what should be a consistent string of 0x020b, 0x5000; 0x022b, 0x5000 would get changed around to 0x50b, 0x0200, 0x052b, 0x0200.
In essence it's swapping nibbles !
My code is really simple and just use delays right now between words. Was leaving the rest for the real programmers.
Just downloaded SP1, but see the SPI master is still v2.4 so doubt anything new there.
Attached pdf show analyzer traces, code, and schematic segment.
Any advice ?
Thanks
Mike S.
- Labels:
-
PSoC 3
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
1. What is the mode of pin 64, your SDAT line seems to have a longer RC time than the SCLK.
2. Did you have anything connected to the SDAT when doing the measurement. Try to have it disconnected and see if that changes.
3. on your pdf file, the first picture shows a small spike on SDAT at the beginning of the 1st packet. Was it from outside circuits?
4. Try to slow down the speed and see if that makes any changes?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi, thanks.
1) SDAT for being bidirectional is set for resistive pull up, also a 10k pull up on it. Zooming up its at 4v at the rising clock edge, so would be more than fine for the slave. Show pics connected and not in attached revised pdf.
2) yes the slave was connected via 2inch flex cable. Removed it and took another pic. Virtually no difference.
3) Didn't give much thought to that transient since out of timing region of interest, figured that was from line tristated then lifted a bit with pull up.
4) Will give going slower a try, but since set for high speed, figured 3Mbps slow enough thats its something else.
Have two other SPI's in PSoc talking to DAC, and digital pot. Don't use them nearly as much, but haven't had known issue.
Tried going from bidirectional to just output, and same outcome.
Attached revised.
Mike
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
1. I think the SDAT should use strong drive, but this is not your problem at this time.
2. for the swaping problem, how about this
Just to see if that changes anything
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks again. Had actually tried that earlier, and no difference. And can't have SDAT as strong drive since need it bidirectional.
Went back to a "working" archive, tested that, and was still working, no upset in SPI transmission.
Updated just the C code to add my new commands, and it works too. Important to note just did BUILD, not clean and build.
Looked into the generated source code for the problem SPI module, and even though both versions set the same, in the working version, the following are NOT enabled:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Opened a case friday, haven't heard back yet.
Have a work around by taking the SPI bidirectional 16 bit and made it one 8bit output only, with a 8 bit shift register to read back.
Numerous clean and builds and still works, just takes a little longer.
Still want to know why, so can go back once the blame thing works right.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Tech support did find an issue with the SPI16.
"The suspected problem is, when you do SPIM_WriteTxDate(0xABCD), initially 0xCD will be written to LSB FIFO and 0xAB is written to MSB FIFO.