Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

I have repeatedly tried to install the package on my XP SP3 box and just at the point where I am informed that the installation has completed, my next click brings up a message telling me that the Update Manager is not installed. The installation apparently terminates with no icons or shortcuts being created save for "CyInstaller for PSoC Designer 5.4" appearing in the Start Menu. How do I get around this roadblock?

0 Likes
7 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

You probably tried installation with admin rights already?

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Yes. My account on my machine belongs to the admin group. This is a one-off anomaly and appears to be bad karma for a particular instance. Everything else works correctly. I have tried the install several times. I'll either figure it out (as I've always had to do with everything else) or just use it on my W8.1 laptop (on which the install proceeded correctly). Thanks for the reply.

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Does the executable appear in its program folder such that you can simply create

   

a shortcut to that ? Not exactly elegant way to do an install but all things else considered

   

might get you up and running.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

The executable is not present. The only application appearing in the program files folder is (incredibly) "psocdesignerinstaller.exe" in the directory tree "Cypress\PsoC Designer\5.4\Updater\". I had a crack at installing 5.4SP1 this evening but maybe I had already tried that particular version as the result was the same. The installer did give me the option to uninstall so that says something.

   

I now have a problem on my 8.1 laptop which didn't come to light until I tried to Build the project (that I finally got to Make successfully on my work machine today after installing 5.4SP1 - had a standard library file-finding issue on this machine prior to today's install/upgrade/repair. I consider that finally being able to program a target device and so complete an assignment to be a matter of good luck Hopefully the object code is free of build/compilation errors. The work machine is a dual-core Win7 box).

   

The error message on my laptop: "*** No rule to make target 'D:\CYPRESS\PSoC1\PSoC'. needed by 'lib/obj/alarm_inv.o'. Stop.  Not very helpful really. This occurred at the Make stage of the process.

   

While I appreciate the modern tools that are being created to make chips as easy to use as possible (and thereby generate silicon sales) it is tempting at times to revert to old ways of doing things - I was writing assemblers 30 years ago. Complexity is not without its drawbacks. I am not a fan of compilers generally.

   

Regards

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Create a MyCase and get in contact with Cypress directly. At top of this page click on "Design Support-> Create a Support Case", leave a link to this thread and your phone number and timezone.

   

Having written compilers myself, I believe in their usability, but a permanently failing installation of an IDE can cost nerves -and coffee 😉

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Hello Malcom Watts,

   

May I create the technical support case on behalf of you regarding this issue? Please confirm.

   

Thanks and Regards,

   

Ramesh B,

0 Likes
Anonymous
Not applicable

Thankyou for your offer. I'm going to try 5.0 SP6 on both machines if I can locate it. The version doesn't really matter so much. It's possible the Windows installer is incompatible. I do have a very early (2006-ish) version of Designer which came with the Miniprog (1?) that works OK and am aware that there may be the odd bug in it. I'm more than half-convinced that the problems are some kind of software clash. It is interesting that 3 machines exhibited 3 different kinds of behaviour with the same version.

   

Regards,

   

malcolm

0 Likes