Dear Cypress engineers:

   

          I have a question about  the psoc creator error,it remind me that:

   

dbg.M0015:Debugger exited unexpectedly during run.Encountered error (Program exited with error :MP3_ERROR)

   

How can i deal with the problem? please let me know the answer as soon as possible,thanks!

0 Likes
6 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Hi,

   

did you change the clocks or did you use sleep or hybernate?

   

This will / can disconnect the debug-session.

   

Bob

0 Likes
Anonymous
Not applicable

Hello Bob :

   

Thanks for you reply, I  also think there are some problems about clock setting in my project, i had modified the clock under the USB clock settings guide,and there was no errors in building process,but when debuging the project ,the error appeared!

   

PS:An ADC conponent and a USB component are included in my project!

0 Likes
Anonymous
Not applicable

hi Jacktan,

   

i haven't encountered such an issue before.

   

can you attach the project in which you were facing this issue?

0 Likes
Anonymous
Not applicable

Do you have a watchdog runnning?

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Hi:

   

Project's .sch design and clock setting is attached for you reference,

   

I had used the watchpoint during the debugging process!

   

Thanks and best regards!

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

attach file!

0 Likes