Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

 Hi all

   

 

   

Simple question - 48 MHz is maximal clock frequency for UDB ?

   

 

   

Thanks info

   

 

   

Kamil

0 Likes
7 Replies
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

No, the UDB can also be clocked with the maximum bus clock. But depending on how you configure it, the maximum frequency can be slower (e.g. for the counters it depends on the bit depth).

0 Likes
Anonymous
Not applicable

 Thanks info

   

 

   

Max bus frequency is same like arm core frequency 67 MHz ?

   

 

   

My idea is very simple verilog VGA controller.

   

 

   

Kamil

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

The Creator timing analyzer will flag you if you have a

   

problem with routes/timing.

   

 

   

Regards, Dana.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Depending on the chip you use the max. Frequency is 80MHz

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

80.01 Mhz.

   

 

   

Regards, Dana.

0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

I raise to 80.02 MHz 🙂 (probably needs hydrogen cooling)

0 Likes
Anonymous
Not applicable

 Thanks help all

   

 

   

My VGA project working fine - 50MHz PLL and about 20% UDB resorces 🙂

   

 

   

Kamil

0 Likes