cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

adpac_1560036
New Contributor II

Hi, im getting the following error pointing to a function call.

   

Build error: undefined reference to `Local'

   

Build error: The command 'arm-none-eabi-gcc.exe' failed with exit code '1'.

   

I couldnt figure it out.

0 Likes
2 Replies
HeLi_263931
Honored Contributor II

Well, 'Local' doesn't exist in the scope where you are referring to it. (And just sending the workspace file, but nothing else, doesn't allow us to look at the sources)

0 Likes
adpac_1560036
New Contributor II

Thank you.!!..The mistake i made was to create  header and source files with the name 'CapSense', which is a default name used by the software. Ive renamed them and now the error is resolved.

0 Likes