PSOC5LP DSI manual routing for 32x32 mux

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
user_294846
Level 3
Level 3
10 replies posted 5 replies posted Welcome!

Hi,

I want to be able to modify the routing for 32 digital signals connected to 32 pins at runtime. All of them output.

User should be able to select which pin has which functionality on the fly.

Implementing this with using the PLDs consumes too much resource (I haven't tried yet but obvious.)

DSI output to pin logic has 4 to 4 mux but I need 32 to 32 mux.

As far as I understand, It's possible with manual DSI routing but the TRM not says enough info about DSI routing.

Is there any document for DSI routing and register details?

Or have you any other resource saving solution for this issue?

IC : PSOC5LP, CY8C5888AXQ-LP096

Thanks, Regards.

0 Likes
1 Solution
Hari
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi user_294846

DSI routing is provided for limited configuration during design time and it is not possible to configure an application like the one mentioned for 32 different routings on the controller.

Thanks and regards
Harigovind

View solution in original post

0 Likes
6 Replies