Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

In working with the FTK, I would like to duplicate the onboard JTAG functionality provided by the CY7C68013A microcontroller. 

   

Why are both SW0IO and SW0CK provided by USBIO (P15_6, P15_7) and PORT1 (P1_0, P1_1) attached to this microcontroller? Which of these two are being used for programming the PSOC5? Could someone with familiarity with the schematic for the FTK and PSOC5 line elaborate this a little further?

   

Thank you.

0 Likes
2 Replies
VivekK_11
Employee
Employee
Welcome! First solution authored 10 replies posted

I just talked to the kit developer about this. Only the Port 1 SWD pins are used for programming in the FTK. The Port 15 pins are present but are not used currently in the kit.

0 Likes
Anonymous
Not applicable

 Thank you very much!

0 Likes