Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

I have a question regarding PLD power draw, particularly digital blocks with a very slow (or no) clock.
I have an application I'm considering porting to PSOC, but before I do I'd like to hear what the consensus is about running PLD blocks in very low power designs.     

 

   

The design needs to sleep for the majority of its lifetime as it is battery powered, and must last several years. the device wakes up roughly once every second for about 1ms, and should have an average power draw below 40uA.     

 

   

I now want to extend the device to incorporate a receiver for a very low data-rate serial protocol. essentially the receiver device will send a wake signal to its micro, followed by a clocked data stream of about 2ms per bit (500 baud). Capturing the data is very easy. In my current micro implementation I sample the data with an interrupt triggered by the clock line. The problem with this is power. As it is currently I have to keep my micro awake for the entire duration of the data transfer (~100ms), which basically kills any aspirations I have for a lower power device.     

 

   

I thought the project might be a good candidate for a PSoC, as I could use an SPI block or even a custom Verilog based block to capture the data, and wake my micro a fixed timeout period after the data has stopped.     

 

   

My question is, will a psoc PLD block draw little enough current if it has a very slow (just the 2ms data clock line, perhaps a 32khz source for timeout...). Can I even have PLD blocks running in sleep modes? Would it be more effective to have the micro simply wake briefly every time the clock line activates?

0 Likes
14 Replies
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Answer is yes with caveats -

   

 

   

    

   

         

   

http://www.cypress.com/?app=forum&id=2233&rID=81146    AN77900

   

 

   

http://www.cypress.com/?rID=78797     AN86233

   

 

   

 

   

Regards, Dana.

0 Likes
lock attach
Attachments are accessible only for community members.
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Graphic did not post, see attached.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

Thanks for the reply.

   

I read the low power app notes again, but they aren't very clear regarding the digital blocks. I noticed the bits in the table about "retention mode" for the UDB blocks, and I'm not really sure if this is simply a consequence of them being utlilsed with a MHz clock (which I can understand will stop) or is there some part of them that is intrinsically disabled? They also refer to 'digital blocks' and Im not sure what they mean by that.

   

let me state it simply:

   

1. If I connect 2 inputs and one output to an asynchronous element like an AND gate and put my psoc in deep sleep, will the AND gate continue to unction as expected?

   

2. If I have a shift register capturing data on one pin, using a clock from another pin (and no other clock source), will it still capture data in sleep/dep sleep modes?

   

3. If I were to power a digital block like a UDB based timer from the ILO clock, will it continue to run in sleep (assuming the ILO is correclty configured to run during sleep)  

   

Thanks in advance for any help. 

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Just a thought, try a quick test, thats the beauty of PSOC you can

   

do a lot of self testing quickly just doing a test project. I agree docs

   

a little thin, you can always file a CASE -

   

 

   

    

   

          

   

To create a technical case at Cypress -

   

 

   

www.cypress.com

   

“Support”

   

“Technical Support”

   

“Create a Case”

   

 

   

You have to be registered on Cypress web site first.

   

 

   

Regards, Dana.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Neither the AND-gate nor the output you may connect the gate to will work in deep sleep.

   

In deep sleep mode only the interrupt controller, ILO, LP-comparators and WDT get powered. (Maybe I've forgotten one or two things like the low-voltage interrupt)

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

PSoC  4000  supports  Sleep  and  Deep-Sleep  modes.  In
Sleep mode, GPIOs are active and  can be actively driven
by  peripherals, such  as  CapSense,  TCPWM,  and  I
2C.  In Deep-Sleep  mode,  pin  states  are  latched  to  retain  the
output  state.  I2C  pins,  however,  are  functional  and  can
wake  up  the  device  on  an  address  match  event.  GPIO
interrupts are available in both the modes.

   

 

   

www.cypress.com/     AN86439

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 Ok, so it seems it could be plausible in normal sleep mode, but not in deep sleep. I guess I'll have to run an experiment when I get the chance.

   

Thanks for the help.  

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Youc an always use a comparator as an AND gate -

   

 

   

Picture of Use Comparator as Logic AND Gate

0 Likes
Anonymous
Not applicable

 Thanks Dana, the AND gate was a hypothetical question. I dont need an and gate.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

You could use an UART for the data transmission which will use 9µA @ 100kBit/s. Wakeup for the transfer could be done with an input pin that gets the PSoC out of deep-sleep. As said before, the GPIO interrupt is still active in this mode.

   

Has somebody already found the specs how much current the PSoC4 draws in deep-sleep?

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

From datasheet -

   

 

   

0 Likes
lock attach
Attachments are accessible only for community members.
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Attached.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

@Dana

   

WHICH datasheet?

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

For whatever reason I thought this whole thread was PSOC 4. So

   

power consumption posted from PSOC 4 datasheet, which is irrelevant

   

to PSOC 5LP.

   

 

   

Regards, Dana.

0 Likes