cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

Just want to know

1) Whether PSOC 5 micro controller CY8C5268AXI-LP047 supports USB host to Pen drive ?

2) Is there any example projects to interface PSOC 5 controller with SD Card.

0 Likes
1 Solution
KyTr_1955226
Valued Contributor

1) PSoC5LP Does not support USB Hosting capability.  I remember hearing rumblings that it might be supported at some point in the future but I have no idea if that's true or not.

2) There's a component for using an SD Card on a PSoC5LP Here and some example code Here

View solution in original post

0 Likes
2 Replies
KyTr_1955226
Valued Contributor

1) PSoC5LP Does not support USB Hosting capability.  I remember hearing rumblings that it might be supported at some point in the future but I have no idea if that's true or not.

2) There's a component for using an SD Card on a PSoC5LP Here and some example code Here

View solution in original post

0 Likes
AnkitaS_51
Employee

Currently, there is no plan to support USB Host capability for PSoC5LP.