cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable
        Is the 3271 Kit Sense and Control Dashboard USB API documented for use in a user developed Host Application?   
   
I want to port an application already developed that uses a high-level USB API. Converting to a Cypress 3271 based system will provide for expansion that the current embedded MCU is not capable of supporting.   
   
I want to avoid having to code a low-level kernel based USB Driver.   
0 Likes
1 Reply
Anonymous
Not applicable
        Now I'm stopping here however this post was too aged. Someone said need the RFCommunicationLib.dll but, Nowhere documentation of it. When import into .NET environment, you can see those class object. I find a PDF from far away. Last part is a sample of usage of APIs.   
0 Likes