Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
DePa_3244516
Level 4
Level 4
First like received First like given

hiii

i have interfaced  CY8CKIT-050 kit and W25Q128Fv flash chip using http://www.cypress.com/documentation/code-examples/ce204087-interfacing-spi-nvram-psoc-35

it works good upto 350kHz frequency but it doesnt work more than that frequency, in the datasheet they have mentioned that it works upto 4MHz

what might the reason behind this?

how can i solve this?

0 Likes
1 Solution
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Watch out to which pins you connected the flash chip (look at the -050 kit schematic). Some of them are used for other peripherals, and some of them even have capacitors attached. This can wreak havoc with the signals.

View solution in original post

3 Replies
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Watch out to which pins you connected the flash chip (look at the -050 kit schematic). Some of them are used for other peripherals, and some of them even have capacitors attached. This can wreak havoc with the signals.

On which pins i have to connect on CY8CKIT-050 kit?

0 Likes

solved it by changing the pins

thank you so much

0 Likes