cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

ETRO_SSN583
Esteemed Contributor

1) Include DDS component in standard library. Super useful component for test

work, generation, etc....

2) WaveDAC component added to PSOC 4M library as a standard component.

Regards, Dana.

0 Likes
1 Solution
odissey1
Honored Contributor II

Dana,

Standard WaveDAC won't work on P4 as it requires 2-byte transfer to IDAC (opposed to 1-byte transfer on P5). There is old demo project showing RAM-DMA-IDAC arbitrary wave generation on PSoC4M, which might be useful:

Re: IDAC with DMA

I wouldn't bet on PSoC standard library updates. It seems like development of PSoC5-type SoCs (programmable hardware + analog) at Cypress is over, shifting towards standard MC design. My guess this is due to the MC market specifics.

/odissey1

View solution in original post

0 Likes
1 Reply
odissey1
Honored Contributor II

Dana,

Standard WaveDAC won't work on P4 as it requires 2-byte transfer to IDAC (opposed to 1-byte transfer on P5). There is old demo project showing RAM-DMA-IDAC arbitrary wave generation on PSoC4M, which might be useful:

Re: IDAC with DMA

I wouldn't bet on PSoC standard library updates. It seems like development of PSoC5-type SoCs (programmable hardware + analog) at Cypress is over, shifting towards standard MC design. My guess this is due to the MC market specifics.

/odissey1

View solution in original post

0 Likes