MiniProg3

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Do i need to purchase a MiniProg3 for an I2C bootloader project?

0 Likes
5 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

As usual: That depends.

   

You need a device with an I2C-interface and the ability to store the project to be downloaded to your application-board.

   

Since your PC does not have got an I2C interface a miniprog3 comes in handy as it contains an I2C-to-USB bridge.

   

Of course you could use a second PSoC-board with a SD-card interface or something similar.

   

You may consider getting a Kit-001 which is more expensive than a Kit -030, but it allows you to develope for PSoC1, 3 and 5 and it additionally contains a miniprog3.

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

There is always the I2C bridge kit -

   

 

   

http://www.cypress.com/?rID=3421

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

ok,thanks.

   

What is the max number of bootloadable applications that can reside in flash in a multi application bootloader project?

0 Likes
Anonymous
Not applicable

 Multiple (Dual) Application bootloader supports a max of only 2 applications in flash.

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

There is nothing to prevent you from modifying a basic boot kernal

   

to accomidate > 2 applications.

   

 

   

Regards, Dana.

0 Likes