Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

 I am trying to test out programming the PSoC5LP dev kit using SWD over the 5 pin interface using the MiniProg3 kit. The PSoC Dev kit board has a 10 pin header for debug and programming, I have been trying to wire up an interface that will allow the programmers 5 pin female molex conector to connect via ribbon cable to the 10 pin port on the dev kit, but my last attempt didn't quite cut the mustard in build quality.

   

I have been able to sucessfully program a board using the 10 pin interface, but for my use, it's very important to reduce pin count and board size so in application we must use the 5 pin interface, and before we roll out our own boards, I do want to have tested this functionality.

   


Does anyone have any sugestions for what I am trying to test out,  perhaps someone has already done this, probaly a much easier way than what I have been doing ?

   

 

   

Thanks!

0 Likes
3 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

PSoC 4 and 5 do not differ much in programming algorithm. So have a look into the schematics of the CY8C49-42xx Prototype board www.cypress.com/ since this can be programmed (I do that frequently) with the 5-pin interface of the MiniProg3.

   

 

   

Bob

0 Likes
JiGi_284761
Level 4
Level 4
Welcome!

Schmartboard has a psoc5 board with a 5 pin SWD. Files are on their website.

   

It would probably be nice if you bought one.

0 Likes
Anonymous
Not applicable

 I will take a look at both of those. Something I have been wondering is that since the MiniProg3 5 pin interface does not have a line for the SWV pin, what limiations does this pose? I understand that I can't do things like serial debug printf, but does it limit the normal debugging experince such as break points and stepping through the code?

0 Likes