cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

ArvindK_86
Employee

Hello Everyone,

   

 

   

Frequency measurements are a common requirement of many applications.

   

 

   

AN2283 - PSoC® 1 Sensing - Measuring Frequency gives a good overview of the many methods that can be used along with their relative error in measurement.

   

 

   

The sample project in the above link, provides an example implementation that is accurate to 0.0016% (16 ppm).

   

 

   

Regards,

   

Arvind

0 Likes
3 Replies
Anonymous
Not applicable

the  sample project  is  very  useful  ,

   

thanks a lot!

   

vincent

0 Likes
ArvindK_86
Employee
0 Likes
ETRO_SSN583
Esteemed Contributor

These are foundation kinds of documents -

   

 

   

Attached.

   

 

   

Regards, Dana.

0 Likes