cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

I currently own a CY8CKIT-059 Psoc 5LP Prototyping kit. I was wondering how accurate the internal timing mechanism aka the on board clock. Also, if there are any recommendation on any crystal oscillator I should look into buying to improve the accuracy of the clock.

0 Likes
1 Solution
Bob_Marlowe
Expert II

The HFCLK accuracy is 1%. See the "Clocks" view in Creator. The LFCLK is can be off to 1000%(!!!), there is already a place on the board to solder a 32768Hz xtal.

Bob

View solution in original post

0 Likes
1 Reply
Bob_Marlowe
Expert II

The HFCLK accuracy is 1%. See the "Clocks" view in Creator. The LFCLK is can be off to 1000%(!!!), there is already a place on the board to solder a 32768Hz xtal.

Bob

View solution in original post

0 Likes