cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

GoKe_1237761
New Contributor II

I need to add a SPIM to my project but my resorces are limited.

The device is a CY8C29666-24PVXI.

I only have DBC 22 and DBC 32 free to use.

I have GOE4,5,6 free.

I have GOO 0 to 7 free.

I have GIO 0 to 7 free.

Port 4 0 to 7 free.

I cant seem to figure out the routing for this device can any one help ?

Thanks

Gord

0 Likes
1 Solution
SampathS_11
Moderator
Moderator

Hello Gord,

SPIM needs an input, MISO. If you want to connect this input to Port 4, you will have to route it through GIEx. You have to reroute other connections so that one of GIEx is free. Otherwise you might have to free up an input in an odd port.

Best regards,

Sampath Selvaraj

View solution in original post

0 Likes
1 Reply
SampathS_11
Moderator
Moderator

Hello Gord,

SPIM needs an input, MISO. If you want to connect this input to Port 4, you will have to route it through GIEx. You have to reroute other connections so that one of GIEx is free. Otherwise you might have to free up an input in an odd port.

Best regards,

Sampath Selvaraj

View solution in original post

0 Likes