- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I'm currently trying to use JTAG EXTEST instruction to characterize a custom component attach to my CY8C5287AXI-LP095 (TQFP 100) without any success
Reading at the BSDL file (CY8C58LPXXX_TQFP100_4JTAG.bsdl) it's written:
This CY8C58LPXXX TQFP100 BSDL file supports 1149.1 testing only after two of the following conditions are satisfied:
1. The JTAG port is enabled.
2. All IOs are pre-configured to drive out fast strong high/low.
JTAG access can be enabled either through programming NV-Latch bits appropriately or through using test-port acquisition protocol. The IOs may be pre-configuration either by writing port configuration registers directly through a test port, or relying on a programmed boot sequence which does that to complete automatically. Testing other IO configurations requires changes to this file and the pre-configured IO configuration.
JTAG is enable by default on chip from factory, and I have successfully achieve accessing IO configuration register and output value register (succesfully toggle a LED) through the jtag chain using programming svf file generated adding access to those register.
However after doing so I'm still not able to use Sample/Preload and Extest jtag instruction.
Does anybody know something I may miss or could provide an example of SVF file achieving this ?
Thanks
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Since you are able to toggle LED JTAG is enabled and also IO port is strong mode. Can you post JTAG command sequence you are using and also error messages if any you are getting ?