cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

HuEl_264296
New Contributor II

We had a problem with a PCB manufacturer. They populated our boards with CY8C3666LTI-201 instead of CY8C3666LTI-027. Now my design won't fit into the chip! I need 5 more 'blocks', (I assume UDBs?).

   

 

   

I'm currently trying to optimise the design, and I'm now only 4 blocks short. However, the error messages aren't that helpful. The UDB is a complex object, and it's not clear exactly what parts of the UDB it isn't able to place. Is it the Datapaths, PLDs, what? As far as I can tell, the .rpt file only reports on the last successful build, and so doesn't give any clue as to why a build failed.

   

 

   

Is there any way I can analyse my problem? What features should I try to optimise? What features might I need to get rid of to fit my design?

   

 

   

103-000-2006-01.cywrk.Archive03.zip

   

 

   

Thanks for any advice.

0 Likes
10 Replies
HeLi_263931
Honored Contributor II

Npo, the report file should have the information from the last build you run. So it shows you were it tried to put stuff, and which resources are used.

   

Were to look for optimization:

   
        
  • usage of fixed-function components instead of UDB components
  •     
  • configuring the UDB components to use less UDBs - for that, look into the data sheet, it shows the resource usage
  •     
  • be careful with glue logic and registers - they might hog resources
  •    
0 Likes
Bob_Marlowe
Expert II

I could come a bit nearer to 2 blocks short by removing the digital-io control registers. that would require a change in program and writing to the pins directly using a shadow register.

   

I am not sure what your ss-logic with the ored outputs is good for, possibly something that can be done in software, too.

   

 

   

Bob

0 Likes
ETRO_SSN583
Esteemed Contributor

Shadow registers apply to PSOC 1, PSOC 3 pin APIs take care of

   

the Read modify Write problem on GPIO.

   

 

   

Regards, Dana.

0 Likes
Bob_Marlowe
Expert II

I was talking about shadow registers to have the ports switched synchroneously which else may affect the external hardware.

   

A Port_1_Write() followed a few µs by a Port_2_Write() may have side-effects I cannot see from the schematic. Since originally the ports are switched simultaneously I thought this to be a safer solution.

   

 

   

Bob

0 Likes
HuEl_264296
New Contributor II

 Bob,

   

 

   

In my design, all of the SS lines which exit the chip are controlled by software. The hardware SS lines from the Flexible_SPI components are ANDed together to detect when they have all finished their transactions.

   

 

   

Please find attached the contents of my .RPT file. What can I learn from it. It doesn't seem to say anywhere that I have exceeded 100% capacity on any particular resource.

   

 

   

Many thanks

0 Likes
Bob_Marlowe
Expert II

You should inspect the .rpt- file from your original (working) design. The .rpt of the non-fitted design does not reflect what did not fit into into the device, but only what fitted so far.
 

   

The difference between your chips is the number of UDBs (24/20). Part of an UDB are 2 PLD (Programmable logic) blocks.

   

The already reduced design (Control Registers) still needs 43 PLD-blocks and only 40 are availlable.

   

When you can reduce some of your used logic you can succeed, some FFs, some gates...

   

 

   

Bob

0 Likes
HuEl_264296
New Contributor II

 When I switch back to the 027 device with 24 UDBs, I can compile the project. This is what the .RPT file says:

   

 

   

Resource Type                 : Used : Free :  Max :  % Used

   

============================================================

   

Digital clock dividers        :    8 :    0 :    8 : 100.00%

   

Analog clock dividers         :    1 :    3 :    4 :  25.00%

   

Pins                          :   47 :    1 :   48 :  97.92%

   

UDB Macrocells                :  111 :   81 :  192 :  57.81%

   

UDB Unique Pterms             :  211 :  173 :  384 :  54.95%

   

UDB Total Pterms              :  224 :      :      : 

   

UDB Datapath Cells            :   11 :   13 :   24 :  45.83%

   

UDB Status Cells              :   17 :    7 :   24 :  70.83%

   

             Status Registers :    1 

   

            StatusI Registers :   14 

   

                   Sync Cells :    7 (in 2 status cells)

   

UDB Control Cells             :   10 :   14 :   24 :  41.67%

   

            Control Registers :    5 

   

                 Count7 Cells :    5 

   

DMA Channels                  :   10 :   14 :   24 :  41.67%

   

Interrupts                    :    3 :   29 :   32 :   9.38%

   

DSM Fixed Blocks              :    1 :    0 :    1 : 100.00%

   

VIDAC Fixed Blocks            :    0 :    4 :    4 :   0.00%

   

SC Fixed Blocks               :    0 :    4 :    4 :   0.00%

   

Comparator Fixed Blocks       :    0 :    4 :    4 :   0.00%

   

Opamp Fixed Blocks            :    0 :    4 :    4 :   0.00%

   

CapSense Buffers              :    0 :    2 :    2 :   0.00%

   

Decimator Fixed Blocks        :    1 :    0 :    1 : 100.00%

   

I2C Fixed Blocks              :    1 :    0 :    1 : 100.00%

   

Timer Fixed Blocks            :    0 :    4 :    4 :   0.00%

   

DFB Fixed Blocks              :    0 :    1 :    1 :   0.00%

   

USB Fixed Blocks              :    0 :    1 :    1 :   0.00%

   

LCD Fixed Blocks              :    0 :    1 :    1 :   0.00%

   

EMIF Fixed Blocks             :    0 :    1 :    1 :   0.00%

   

LPF Fixed Blocks              :    0 :    2 :    2 :   0.00%

   
        
   
        
0 Likes
HuEl_264296
New Contributor II

 Where in the .RPT file can I see the number of PLDs used?

0 Likes
ETRO_SSN583
Esteemed Contributor

From -               http://www.cypress.com/?rID=69773

   

 

   

PSoC UDBs
PSoC implements programmable logic  through an array of
small,  fast,  low-power  digital  blocks  called  Universal
Digital Blocks (UDBs).  PSoC devices have as many as 24
UDBs. As shown in Figure 1,  a  UDB consists  of  two small
programmable  logic  devices  (PLDs),  a  datapath  module,
and status and control logic.

   

 

   

Each UDB you place lists the resources it uses in the datasheet

   

for that component,

0 Likes
Bob_Marlowe
Expert II

"Where in the .RPT file can I see the number of PLDs used?"

   

A little bit further down, look (or search) for "PLD Packing Summary"

   

 

   

Bob

0 Likes