How shall i can generate an interrupt on the falling edge of a Comparator?
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
Hello Everyone,

   

I want to fire an interrupt on the falling edge of the comparator. I directly attached an interrupt source to a comparator(see attachment), but it only has a rising edge option.

   

I don't really understand the option "LEVEL".

   

Looking forward for your help!

   

Regards

   

Awais

0 Likes
10 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Set the polarity of the comparator to "inverted".

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Thank you, Bob, for your reply.

   

Sorry, One information is missing : I want to generate the interrupt on the rising and falling edge of the comparator.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Use an inverter and two isrs. Does that work?

   

 

   

Bob

0 Likes
Anonymous
Not applicable

I haven't tested that. 

   

But I think it will not work! Because according to datasheet:

   

Inverting: Output goes high when the positive input is less than the negative input.

   

Non-Inverting (default):  Output goes high when positive input is greater than negative input.

   

Also the question is, how the ISR will know when the falling edge of the signal is there? because if we see in the properties of the isr, it has three options, derived, rising and level.

   

I have no idea about "level".

   

Awais

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Are you using comparator v 1.20? If not, update!!!

   

 

   

Bob

0 Likes
Anonymous
Not applicable

No, Its 2.0

   

 

   

Awais

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Update!!!! Are you using Creator 3.3 CP3 (Creator -> Help -> About) If not, update first Creator to latest!!!

   

 

   

Bob

0 Likes
Anonymous
Not applicable

I updated all components. But I think v 2.0 is the latest one.

   

Yes, I am Using PSoC Creator  3.3 SP2 (3.3.0.9604).

   

Awais

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Sorry, my fault. I was on PSoC4 which has a different comparator. So you need to connect two isr components to the comparator output and the inverted comparator output using a NOT gate.

   

0 Likes
Anonymous
Not applicable

Ahan!

   

Ok, I will try this 🙂

   

Thankyou Bob

0 Likes