cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

rjjong1
New Contributor

Hi,

I have trouble programming the CY8C29666-24PVXI. I am using the PSoC Programmer 3.29.0 and can't select the CY8C2xxxx Device Family. There is no option there. Do I have the right software to program the microcontroller, or do I need to install something else?

0 Likes
1 Solution
SampathS_11
Moderator
Moderator

Connect a MiniProg or MiniProg3 and start PSoC Programmer. Kindly put the Programmer in "ISSP" mode in the "Programmer Characteristics".

Then, select disconnect the MiniProg, from the "Port Selection" box on the top right. This will enable "Device Family" and "Device". Select "29x66" in the "Device Family" and then "CY8C29666-24PVXI" in the "Device" selector.

SampathS_11_0-1616492013898.png

Best regards,

Sampath Selvaraj

View solution in original post

0 Likes
1 Reply
SampathS_11
Moderator
Moderator

Connect a MiniProg or MiniProg3 and start PSoC Programmer. Kindly put the Programmer in "ISSP" mode in the "Programmer Characteristics".

Then, select disconnect the MiniProg, from the "Port Selection" box on the top right. This will enable "Device Family" and "Device". Select "29x66" in the "Device Family" and then "CY8C29666-24PVXI" in the "Device" selector.

SampathS_11_0-1616492013898.png

Best regards,

Sampath Selvaraj

View solution in original post

0 Likes