cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

WaMa_286156
Contributor II

I have created a small FreeRTOS project that can be expanded.

Project status:

1)  CY8CKit-059 targeted

2)  Uses 32K RAM (can be changed)

3) Uses Micro-USB as a USB-Uart.

4) Uses the Finger Stick Debugger USB-Uart port (if not broken off), otherwise uses UART to pins 12[6],12[7]

5) Starts flashing blue User LED when powered on.

6) Easily debugged using PSOC Creator.

Enjoy!

1 Reply
Rakshith
Moderator
Moderator

Hi WaMa_286156​,

Thank you for sharing your project with the community

Best Regards,

Rakshith M B

Thanks and Regards,
Rakshith M B
0 Likes