cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

BUTA_1301626
New Contributor II

I've reviewed your sample Filter_ADC_VDAC01 project.I also watched the video. I made it in the video file.but the filter does not work as shown in the video.I increase the frequency of the function generator from 1kHz to 7kHz. I see the same signal on the oscilloscope at the output.Normally I should not see the sign on the output after 6kHz.I could not find where I made the mistake.I use Cy8ckIt-050.I am sending a file attachment.

0 Likes
1 Reply
EmHo_296241
Contributor II

Hi,

Can you share the link to the video you have referred ?

0 Likes