Error n connecting resistor
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
I am facing the problem in connecting the resistor  to the circuit ...i send the pic of the circuit and the error too...plz provide some information in how avoid that error.....

0 Likes
2 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Since your resistors are external parts (as all annotation components are) you have to connect them via pins to the outer world.

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Are you trying to build a simple OpAmp summer ? If you don't need

   
   

the hi Z afforded by the PGAs you can always eliminate them. And

   
   

take your gain individulally for each channel by picking specific input

   
   

resistors. Also offset the OpAmp so circuit works with - values.

   
   

 

   
   

     http://www.ecircuitcenter.com/circuits/opsum/opsum.htm    

   
   

 

   
   

Right now your circuit has a gain of - 1 in the OpAmp summer, referenced to ground,

   
   

hence will not work, eg. output of OpAmp cannot swing below ground w/o you offsetting

   
   

the NI input from something higher than Vss.

   
   

 

   
   

Note dropping PGAs has the additional advantage of less offset and drift. If

   
   

you still need super high Z inputs, have to use PGA, you still have to offset the

   
   

OpAmp.

   
   

 

   
   

Regards, Dana.

0 Likes