cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

Hi,

   

I measured that the time for execution of the EEPROM_Write function is ca. 15 ms, which is far away from the typical value of 2 ms specified as "Single row erase/write cycle time". Is that possible or does this function have so much overhead time because it is doing a single row erase and write ?

   

BTW, I used the CySetTemp() function to compensate for temperature influence.

   

Thanks 

0 Likes
1 Reply
ETRO_SSN583
Esteemed Contributor

From CY8C58xx datasheet -

   

 

   

   

 

   

Regards, Dana.

0 Likes