Dynamic Reconfiguration

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello everyone,

   

I have a quick question how to reconfigure the (analog) part of the PSoC 5 in a running program.

   

For Instance:
I want to change the output range of an IDAC from 0-32 µA to 0-2,04 mA. I want to use the same DAC, only in a part of the program the range should be changed.

   

Another thing is to reassign pins during a program. How can I do that?

   

To myself: I am a student using the PSoC 5 and just started working with PSoCs. I found the application note on dynamic reconfiguration, but it is only for PSoC 1.

   

Thanks in advance for your help,

   

Thomas

0 Likes
1 Solution
Anonymous
Not applicable

Hi Thomas,

   

 

   

IDAC in PSoC 5 supports 3 output ranges. In order to change the range from 0-32 µA to 0-2,04 mA, the API IDAC8_SetRange(uint8 range) can be used.

   

The parameter "range" can be IDAC8_RANGE_32uA or IDAC8_RANGE_255uA or IDAC8_RANGE_2mA as per your requirement.

View solution in original post

0 Likes
1 Reply
Anonymous
Not applicable

Hi Thomas,

   

 

   

IDAC in PSoC 5 supports 3 output ranges. In order to change the range from 0-32 µA to 0-2,04 mA, the API IDAC8_SetRange(uint8 range) can be used.

   

The parameter "range" can be IDAC8_RANGE_32uA or IDAC8_RANGE_255uA or IDAC8_RANGE_2mA as per your requirement.

0 Likes