cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable
        I have dynamixel motor (http://www.electronickits.com/robot/BioloidAX-12(english).pdf) and CM900 kit. I want to drive dynamixel motor with psoc3. There is ttl communication on the cm900 kit. Maybe I can communicate psoc3 but I do not know how to write a c code. How can I do that?   
0 Likes
2 Replies
Anonymous
Not applicable
        HI I'm looking through the PDF. Communication that will do by Half duplex UART with TTL level interface.. So you have to use the UART module and connect directly. Regarding software, you submit instruction packet and will get status packet from the motor. There are sample program list in there, you can use it to meets psoc program code. It is not hard, I guess so. Thank you.   
0 Likes
ETRO_SSN583
Esteemed Contributor

You could always drive the servo directly from PSOC, eliminating

   

dynamixel board. You need a power driver interface, or discretes

   

to handle the currents.

   

 

   

Regards, Dana.

0 Likes