cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

 Hi all, 

   

Greetings,

   

I'm trying to design my own application board using PSoC 5lp.  All the functionalities of the new board are :

   

1) Cy8C5868 chip can work well

   

2) It can be programmed by Miniprog3

   

3) It can connect to PC using USB

   

4) connectors for at least 32 GPIOs

   

5) Powers

   

In addition, I used development kit to test my application before.   I read the schematic of Develpment kit (attached here). But it contains a lot extra modules that I don't need. Sadly,  I can't totally understand some modules.  Are these parts below necessary for my new design:

   

1)Voltage Reference

   

2) Protection circuits

   

3)Internal Boost Regulator

   

Could you please also tell me the main function of these parts? 🙂

   

Also, I will appreciate any suggestions from you about how to design the new board. 

   

Thank you so much!

0 Likes
5 Replies
ETRO_SSN583
Esteemed Contributor

1)Voltage Reference

   

 

   

Thats internal in PSOC unless you wanted to use an external reference. Allow

   

for the option to bypass to a fixed pin the internal reference to minimize ref

   

noise at high resolutions. There is a dedicated pin for this use to implement

   

the Vref bypass.

   

 

   

2) Protection circuits

   

 

   

To protect pins from transients that try to take pin > Vdd + .5 or < Vss - .5.

   

These transients can cause latchup of PSOC or at least unpredictable

   

operational faults.

   

 

   

3)Internal Boost Regulator

   

 

   

For operation on singler cell battery applications, or very low voltage rail

   

that you need to boost to allow PSOC to run at a higher voltage.

   

 

   

Regards, Dana.

0 Likes
ETRO_SSN583
Esteemed Contributor

Some useful references -

   

 

   

    

   

          

   

http://www.cypress.com/?rID=43337     AN61290 - PSoC® 3 and PSoC 5LP Hardware Design Considerations

   

 

   

    

   

          

   

http://www.cypress.com/?rID=39677     AN57821 - PSoC® 3, PSoC 4, and PSoC 5LP Mixed Signal Circuit Board Layout Considerations

   

http://www.cypress.com/?rID=40247     AN58827 - PSoC® 3 and PSoC 5LP Internal Analog Routing Considerations

   

http://www.cypress.com/?rID=39974     AN58304 - PSoC® 3 and PSoC 5LP – Pin Selection for Analog Designs

   

 

   

Regards, Dana.

0 Likes
JiGi_284761
New Contributor

Use a board with 2 mill copper so you can replace the parts you burn out. Use single sided board.

   

Use a separate 5 volt and 3.3 volt regulator and put current limiting resistors in line. You will most probably use components with different voltage levels.

   

Put current limiting resistors or use opto couplers on all IO. This is where you will fry most parts. 

   

Get in the habit of using cable connectors that are shrouded. A DB25 connector  on the board with a plug that has removable pins works well and is durable.

   

Some boards can be hard to program if there is already a program running that uses IO such as PWM or I2C or something of the sort so if you can put headers and jumpers on all io pins.

0 Likes
Anonymous
Not applicable

Hello Dana,

   

Thank you for your clearly explaination about those parts. Also the materials are also useful. 

   

Best Regards,

   

Mary

0 Likes
Anonymous
Not applicable

 Hello SCAS,

   

Thank you for helping me!

   

You suggested using a separate 5 volt and 3.3 volt regulator. I get confused for this part.  Could I only design 3.3 volt power for my board. Is 5 volt necessary? Thank you:)

   

Best Regards,

   

Mary

0 Likes