cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

How can the 'configurable reset' pin P1[2] configured as reset? Can't seem to find it anywhere...

   

(This is for the CY8C5588 processor board, on the CY8CKIT-001. )

   

Thanks,

   

~Abhijit

0 Likes
5 Replies
Anonymous
Not applicable

Hi Abhijit,

   

 

   

Since you are using 100 pin CY8C5588 part, you can enable Optional XRES on P1[2] by selecting the same in the System tab of the .cydwr file.

   

It can be found at the following location:

   

.cydwr file > System > Programming / Debugging > Use Optional XRES

   

 

   

 

   

The snap-shot below shows the setting done.

   

 

   

   

 

   

 

   

 

   

Regards,

   

dasg

0 Likes
Anonymous
Not applicable

Found it.. thanks.

   

~Abhijit

0 Likes
Anonymous
Not applicable

Hi,

   

I would enalble the optional reset but I can't find that option in the programming\debugging menu.

   

I use PSoC Creator 2  and I see only two options:

   
        
  • Debug Select
  •     
  • Enable Device Protection
  •    
   

I use a CY8C5588AXI-060.

0 Likes
Anonymous
Not applicable

The optional XRES input (p1[2]) is no longer supported and has been disabled (it is no longer presented in the System design-wide editor). 

0 Likes
Anonymous
Not applicable

This feature has been disabled for PSoC5 in PSoC Creator 2.0

0 Likes