Announcements
IMPORTANT: Cypress Developer Community currently doesn’t allow sign-in to prepare for the upcoming transition. To learn more, check out our announcement.
cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

I'm trying to automate loading of firmware on a device via SWD. In order to do so, I'm running the CLI tool from a Windows CMD prompt. Everything starts fine but when I try to "Program" the device I get this error:

   

"Device is not in ISSP mode"

   

I try to set the device to program via SWD (SetProtocol 😎 but this does not seem to work. Is there some kind of trick I need to use to get this to work? The process works fine from the PSoC Programmer UI. When I try to script the process using the "runfile" command rather than typing into the CMD prompt I get the same error.

   

EDIT: This is with PSoC Programmer 3.24.4

0 Likes
7 Replies
Bob_Marlowe
Expert II

Welcome in the forum, rob.

   

Although I do not know if it will cure your issue, I would recommend to update to Creator 3.3 CP3 which is the actual latest version. Do not forget to update your project's components as well.

   

 

   

Bob

0 Likes
himam_31
Employee

Hello,

   

Can you send us the series of commands and the output for the commands that you executed before performing "Program" command.

   

Thanks,

   

Hima

0 Likes
Anonymous
Not applicable

Recently I encountered the same problem. I cannot acquire device (PSoC4) in SWD mode with neither Miniprog3 or KitProg. Additionally for Miniprog3 I have to choose a different type of connector. I use a 5-pin connector. But to power up the processor I have to use the "SetProtocolConnector 1" command, despite the fact that psoc_programmer_cli.pdf says that for SWD mode parameters are
 0 - 5-pin connector
 1 - 10-pin connector

   

With GUI applications all is programmed correctly with the Miniprog3 or KitProg

   

Miniprog3 cmd:

   
version <version 3.25.0 1 OK GetPorts <MiniProg3/1443DD00051D KitProg/0F20083201324400 0 OK OpenPort MiniProg3/1443DD00051D . < 0 OK GetProgrammerCapabilities <0x0007-0x0007-0x0001-0x0002-0x002f-0x000f 0 OK SetProtocol 8 < 0 OK SetAcquireMode Reset < 0 OK PowerOn < 0 OK SetPowerVoltage 3.3 < 0 OK SetProtocolConnector 1 < 0 OK Acquire E Device is not in ISSP mode. Acquire returned 80004005 80004005 OK quit <OK <OK
   

 

   

KitProg cmd:

   
version <version 3.25.0 1 OK GetPorts <MiniProg3/1443DD00051D KitProg/0F20083201324400 0 OK OpenPort KitProg/0F20083201324400 . < 0 OK GetProgrammerCapabilities <0x0001-0x0006-0x0001-0x0000-0x000c-0x0000 0 OK SetProtocol 8 < 1 OK Acquire E Device is not in ISSP mode. Acquire returned 80004005 80004005 OK quit <OK <OK
0 Likes
Anonymous
Not applicable

I'm with the same situation that I can DAP_Acquire and I can read Flash information but Program always returns "Not in ISSP Mode"

0 Likes
Anonymous
Not applicable

Is there a solution to this issue because I see the same when programing with the Psoc GUI there is no problem but thru CLI interface the programmer always return: Device is not in ISSP mode

0 Likes
Bob_Marlowe
Expert II

See the different modes of the Kitprog in its manual. Watch the LED. Try pressing Reset button on Kitprog for more than 5s.

   

 

   

Bob

0 Likes
BrLa_1334046
New Contributor

 have you checked if your SWD lines are high by default? You may have to add a pullup resistor on swdclk and swdio. I am not certain what values of resistor to use but ARM suggests 100k ohms.

0 Likes